如题,想确认下。如果想用外部晶振是不是直接输入到PCLK PIN
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
不知你具体指的什么意思,在使用中频率变化吗?PCLK能支持的频率范围为5MHz~85MHz。
我具体说下状况吧:在这个CASE中,是用925的自带画面传输到928,然后928传输到TFT显示。主要目的是为了模拟外部信源输入给928工作的状态,由于屏有CLK要求,需要在51.2-57M之间。
现状是:925的内部CLK理论上是200的分频,但实测中发现,4分频之后的频率才46.8M(测试928 LVDS CLK OUT的频率),这是不能满足规格的,因为要用来EMC实验,频率的不同结果会相差很大,因此希望频率能在55M左右,以此来验证产品的EMC性能。
想请问有什么好的方法让928的输出LVDS CLKOUT是55M吗?
思路:1、设置925寄存器,用外部CLK模式,PCLK输入调整为55M,所以才会有之前提问:PCLK是可以由外部输入,然后影像源用自带的画面,这样是可以正常工作且达到我的目的的吗?
2、TI是否有可以调整内部CLK的方法?还希望解答
你提到的第一种方式可以实现. 0x14 register bit [2:1] set to 00, external clk input.
model_sel set LF_MODE to 0 frequency range is 15 – 85 MHz (Default)