Other Parts Discussed in Thread: ISO1050
1,参考电路里说,ISO1050和C2000连的时候要加一个RC滤波器,还给了公式,我想请问下,这个滤波器是一定要的么?加了它带来什么好处,还有要用的是别的单片机而不是c2000,是不是也需要加这个呢?
请问下,我是终端电阻120欧,通信速率是1M,那么这两个电阻各为60欧,那这个电容的大小是多少?有没有什么公式得出?在1M的通信速率下
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Other Parts Discussed in Thread: ISO1050
1,参考电路里说,ISO1050和C2000连的时候要加一个RC滤波器,还给了公式,我想请问下,这个滤波器是一定要的么?加了它带来什么好处,还有要用的是别的单片机而不是c2000,是不是也需要加这个呢?
请问下,我是终端电阻120欧,通信速率是1M,那么这两个电阻各为60欧,那这个电容的大小是多少?有没有什么公式得出?在1M的通信速率下
你可以参考下CAN总线的设计指南,里面提到了滤波器设计的计算公式:
R*C=0.032/fs,如果CAN的data rate为1Mbps(500Khz),带入公式60*Csplit=0.032/500KHz,得到Cplit的值。