Part Number: TCAN1145-Q1
电路方案是1145 VIO端口供电为3.3V,与MCU供电为统一电源。
由于MCU可能会涉及到断电复位重启,即3.3V电源会掉电一段时间。那么此时,CAN收发器在3.3V断电时会处于什么状态?休眠还是?会不会进入休眠状态使INH引脚进入高阻态使电路其他电源关闭。
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Part Number: TCAN1145-Q1
电路方案是1145 VIO端口供电为3.3V,与MCU供电为统一电源。
由于MCU可能会涉及到断电复位重启,即3.3V电源会掉电一段时间。那么此时,CAN收发器在3.3V断电时会处于什么状态?休眠还是?会不会进入休眠状态使INH引脚进入高阻态使电路其他电源关闭。
您好,1145 内部集成了欠压保护电路, 包括Vsup,VCC以及Vio三个电压的欠压保护。
如果 Vio降至 UVio欠压检测以下,则禁用多个功能。收发器都会关闭,然后从总线中脱离,直到 VIO 恢复。当 UVio 触发时,tUV 计时器启动。如果计时器超时
UVio欠压仍然存在,则器件进入sleep模式。一旦进入睡眠模式后,需要一个唤醒事件来将 TCAN114x-Q1置于待机standby模式并使能 INH 为高电平。
具体可参考数据手册中10.4.7.6.2中UVio的描述: