我想用DM8168做cPCI总线上的主设备,怎么实现?
怎么将MD8168的PCIe转成cPCI(主设备)使用啊?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
XIO2001是1x的PCIE到PCI的桥芯片,如果你要转cPCI,还得需要PCI到cPCI的adpter card,http://www.connecttech.com/pdf/PCI_to_cPCI.pdf
PCI和cPCI的电气特性相同,但cPCI支持热插拔的功能,而PCI不能,因此直接走线到cPCI上是不能满足cPCI信号的功能的,所以先需要PCIE转PCI,然后加上PCI到cPCI的adapter card,还得需要能够支持热插拔的芯片才能完成cPCI的功能。
PCI和cPCI的电气特性是相同的,如果不需要支持热插拔,直接连线应该是可以的,但最好还是试验一下看下信号质量如何。