请教一下,DP83640用作100M-FX模式时,FX_SD信号如何应用,芯片手册上只是说信号检测,那能不能详细说明一下:
1、FX_SD信号低于多少伏认为无效,高于多少伏有效,
2、在FX_SD无效的情况下,是不是链路灯不会点亮,和MAC接口即使有数据也不会转到链路上去?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
请教一下,DP83640用作100M-FX模式时,FX_SD信号如何应用,芯片手册上只是说信号检测,那能不能详细说明一下:
1、FX_SD信号低于多少伏认为无效,高于多少伏有效,
2、在FX_SD无效的情况下,是不是链路灯不会点亮,和MAC接口即使有数据也不会转到链路上去?
Vih(min)=2V ,Vil(max)=0.8V (Vcc=3.3V); Vil(max)=0.7V(Vcc=2.5V). 也就是说,当高于2.0V时为高电平,当低于0.8V或低于0.7V时为低电平。
1、FX_SD的信号只是检测电平输入吗?当DP83640与HFBR5803光模块配合时,将HFBR5803的SD信号接至DP83640的FX_SD信号,DP83640的链路灯能够根据FX_SD信号指示正确。我用万用表测试,在光纤链路通时FX_SD=2.2V,光纤断掉时FX_SD=1.4V。但当DP83640与HFBR57E5光模块配合时,将HFBR57E5的LOS信号取反接至DP83640的FX_SD信号,DP83640的链路灯就不正确了。我用万用表测试,在光纤链路通时FX_SD=3.3V,光纤断掉时FX_SD=0V。这显然与手册上说的对应不上啊
2、FX_SD的信号有效无效,会影响DP83640的收发工作吗?
FX_SD这个引脚高有效,就是用来检测信号是否有效的,如果FX_SD无效,就不能进行收发工作了啊。
可以看一下这个文章
http://www.union-rnd.com/dp83640%E8%8A%AF%E7%89%87%E5%90%8Csfp%E5%85%89%E6%8E%A5%E5%8F%A3%E6%A8%A1%E5%9D%97%E8%BF%9E%E6%8E%A5%E5%87%A0%E7%82%B9%E6%B3%A8%E6%84%8F%E4%BA%8B%E9%A1%B9/