This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Question about DS90UB9724 usecase



Hi, TI experts

As D/S decribed in 7.3.4.11 CSI-2 Replication, We can see CSI-port0 can support replicate lane0/1 to CSI-port 0 lane2/3 and CSI-port 2 can support replication from CSI-port0/1.

We have questions below:

1. To make sure two host and one serializer can receive 4 camera mipi data.Can we enable CSI-port 2 replication(replicate from CSI-port 0) at the same time?  

2. If CSI-port 0 is configured as C-phy,  is CSI-port 2(only D-phy mode) able to replicate from CSI-port 0

3. About I2C0 and I2C1, do we need to switch the ownership to avoid conflicts (two host access 9724 or remote device at the same time)?