This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
如题。手册上查不到,那这两个DIR和/OE信号的高电平分别是多少?
你好,根据手册的page5,DIR和OE都是通过上拉一个电阻到VCCA,所以高电平都是满足VCCA工作电压的VIH的.
比如如果VCCA=4.5~5.5V时 ,DIR和OE的高电平输入电压最小应该为2V.
我在网上下的一个资料,英文的,只有8页,在P5没有您说的这样的图,麻烦能否往我的邮箱发一份新的datasheet?谢谢了先
你好,相关的解释是文字描述,手册中的PAGE1也有提到,DIR和OE是通过电阻上拉到VCCA,如果输入电压>2V时就满足高电平的要求
http://www.ti.com/cn/lit/gpn/sn74lvc4245a
我看的资料版本低,在新版本的资料里看到了。谢谢!
以后看TI产品的datasheet,可直接在官网上右上角输入产品型号,进入其产品主页之后都是最新版本的参考资料。
http://www.ti.com