This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
为了应用CDCE421A芯片,买了评估板,刚收到货,CDCE421A Control GUI v 1.0.msi这个软件在win7系统下能正常工作吗?安装过之后打开,老是提示Error installing Driver ! Error 5,这是怎么回事?另外评估板的B block区的贴片时钟是多大?贴片时钟上 字符为 320 ABMME 4Q,是压控的吗?
我在win 7上试了一下,果然情况和你的一样,也是出现类似的错误,但是点击OK之后好像也是可以用的,另外,关于这个error的产生,我们也会进一步核实。
根据CDCE421A EVM use's guide中给出的B block采用的是AT crystal(电路图中给出的xxMHz),这是因为 AT crystal的频率的值可根据欲得到的输出频率的值来计算的,这个在CDCE421A的datasheet Page7有解释,比如如果想实现622.08MHz 的输出,那么根据公式2,选择VCO1,输出分频系数为1,预分频系数为3,反馈分频系数为20,得到AT crsytal的频率值为1/20 Vout=(1/20)*622.08Mhz=31.154MHz.
一般的EVM的user's guide中都会给出BOM表,奇怪的是CDCE421A这块板子的user's guide中没有给出。你是通过哪家代理商购买的?看联系下代理商是否有EVM板的BOM表可以提供。