Other Parts Discussed in Thread: TXB0108
原理图如下:
从A侧输入的信号如下:
放大后如下:
在B侧输出的信号如下:
放大后如下:
A侧的输入信号电平是3.3V,正常情况下,B侧输出应该是电平为5V,现在输出在2V上下小幅震荡,请问是哪里出了问题?(未用到的通道引脚都接地了)
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
有三点需要注意:
第一,TXB0108不适用与像I2C这种OD架构的应用。
第二,信号的data rate为多大?TXB0108的最大data rate能支持100Mbps。
第三,检查下A端输入信号的电流是否能达到2mA,TXB0108对输入要求:
For proper operation, the device driving the data I/Os of the TXB0108 must have drive strength of at least ±2 mA.
那你量一下OE信号的波形吧,从VCCA上电开始到VCCA达到稳定3.3V时的一个波形,因为OE为高有效,Vih(min)=0.65VCCA,否则输出为高阻抗状态。