This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TCA9539

Other Parts Discussed in Thread: TCA9539

TCA9539 最大工作电流为 ICC 为 160mA ,请问这为 VCC最大输入时的电流吗,

现在需要 TCA9539 的最大功耗值,即最恶劣情况下芯片能承受的功耗,包括电流和电压

清帮忙确认 160mA,  -200mA 的条件,谢谢!

 

  • 你好,

    手册14页的下面第三个注释有说明一些信息。这个160mA是极限参数,你的IO输出电流总和要控制在这个范围内。

  • Icc指的是流经Vcc端的电流,指的没有输入信号时器件本身的静态电流,也就是TCA9539自身的功耗。

    如果你需要最大功耗,这个功耗应该是器件本身的静态功耗+输出功率。在TCA9539的datasheet中给出了最大输出钳位电流为20mA,如果电压为Vcc,那么总的功耗为=(Vcc*160mA)+N*(输出电压*20mA),其中N代表了如果输出为多通道的。

x 出现错误。请重试或与管理员联系。