我们方案中,信号从DS90UB925Q传送到DS90UB928Q,用双绞屏蔽线,长度1.8m,在EMC实验中,RE会有很多频段NG,测试发现辐射从传输线上出来,想请问,LVDS信号不是比较弱吗?辐射值为什么会比较严重。
LVDS本身的信号有没好的处理建议?试过加电容,10PF,但传输速率这很快,最高有1G,加电容不好吧?而且也没什么效果
线材上,是USB用的线,双绞+屏蔽,还有没有更好的线材推荐?线材需要和PCB LAYOUT一样做差分阻抗匹配100欧吗?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
线材推荐使用100ohm双绞屏蔽线。此外,可以尝试PCLK增加展频功能看EMI是否有改善。
PCLK允许展频,925可接受到35K ±2.5%的三角调制展频信号,925本身对PCLK在f/40到f/20之间的抖动还是有要求,规格书上有提及。
阻抗匹配不好的话是有可能导致EMC的问题的,你可以尝试在线上串接几个ohm的电阻试下。