AM26LS31上电后会发烫,而且会越来越烫,供电电压是5V,输出和输入什么都不接也是这样的情况,请问为什么?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
通过datasheet中给出的电气参数可知,当vcc=Max=5.25V 时候,静态电流的范围为32mA~80mA,你测得的54.5mA在这个范围之内,那就是正常的。
发烫就是功耗大,对于AM26LS31来说,一是本身没有散热焊盘,二是静态功耗也比较大,所以如果想降低功耗,要么改换其他热阻小的产品,要么就是如果在不用的时候,可以将输出disable掉,减少输出功耗。
可以考虑DS26C31这款,也是422的四路驱动器,5V供电,但这款的静态电流只有0.2mA,相对AM26L31的32~80mA来说,静态功耗小很多。