Other Parts Discussed in Thread: CDCE62005
我在配置CDCE62005时,配置完9个寄存器后,启动手动自校验后无法抓到上升沿,我采用的25MHz差分晶振输入,输出频率为50MHz和20MHz。经过配置后我能够得到正确的输出频率值,但是PLL无法锁存。下面是我配置的寄存器值:
E904 0320 //register0
E904 0301 //register1
E90E 0302 //register2
E90E 0303 //register3
E80E 0314 //register4
5000 8A75 //register5
84AE 0106 //register6
BD9A 3DF7 //register7
2000 5FF8 //register8
在写完这9个寄存器后我等待了500us后将寄存器6再次写入(仅改变bit22=0),然后再次写入寄存器6(仅改变bit22=1),在整个过程中都无法抓取到pll lock信号的上升沿。请大神指教是什么原因?