This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
需要1驱8的时钟buffer,用于AD/DA,需要skew和jitter都尽量小,时钟频率大概300M左右,有推荐的吗,谢谢了。
看你是什么电平了。LVDS的可以用CDCLVD1208,LVPECL的可以用CDCLVP1208.都是1:8的buffer
需要和你确认几个问题,以便帮你选型,你是需要差分输入,单端输入?输入电平是CML,LVPECL,LVDS或者LVCMOS?供电电压多大?以及需要几个通道的?
比如CDCLVD2108这款1:8 fanout器件,就是一款双通道的 1:8 Differential Buffer,输出为LVDS电平,输入为LVDS, LVPECL,或LVCMOS都可。
谢谢耐心和详细的回答。
我需要差分输入,电平是LVDS,供电电压2.5或者3.3都可,8通道输出。目前我选了LMK01010这个器件,jitter和skew都很小,这个输入时ac耦合,应该支持lvds输入吧。