Other Parts Discussed in Thread: DS90UB933-Q1EVM
图像传感器-----DS90UB933-------DS90UB934,这样的连接方式,使用同轴电缆来连接。并且933的PCLK来自图像传感器。频率为96MHz。现在观查到的现象是,在934端,可以用示波器观察到
HSYNC和VSYNC,这2个信号的频率和设定的传感器输出是对的上的,而且低电平是0V,高电平1.8V和934的VDDio一致。但是PCLK有问题,示波器截图如下。
,可以很明显看到低电平的时候不是0V,好像被一个直流电平抬升了。但是在原理图中,934的PCLK是直接输出到其他板子上的,没有连接其他东西,这个截图是在拔掉与其他板子的连接线测得的。这个现象很奇怪。这个波形和图像传感器的晶振很像。我的图像传感器接的是96MHz的外部有源晶振,并且在图像传感器里,设定为外部晶振直接输出到PCLK。这样的应用会有问题吗?