Other Parts Discussed in Thread: TVP7002, THS8200
TVP7002有没有设置DE和数据自动对齐的功能(即分辨率最左边的第一个像素与DE对齐)?
现在发现有个别分辨率的数据提前于DE信号几个时钟周期;
如果VGA信号经过VGA分配器等设备,在接入TVP7002后,则大部分都存在有效数据相对于DE信号有延迟。
现在的应用需要根据DE信号采集有效数据,如果无自动对齐功能,那就需要针对不同分辨率,不同应用场手动校准对齐,很麻烦。
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
你的这个问题很可能是同步没做好,跟HSYNC和VSYNC的设置有关,楼主可参考下面这个帖子,这个帖子几乎包含了所有TVP51xx系列以及高清AD TVP7200和DA THS8200经常遇到的问题,相信你看了之后一定有所收获,有关TVP7002常遇到的问题,可参考5楼的贴:
你的意思是目前DE 信号对齐的并非是有效数据,是那些没用的消隐信号,你可以看下TVP7002的寄存器,0x17h,bit[6:4]设置成001,为Data Enable output,bit[0]output enable 配置成0使其使能,这时候data enable对应的输出便是有效的数据。请看下面注释:
NOTE: Data Enable output is equivalent to the internal active video signal that is controlled by the AVID start/stop pixel
values and the VBLK offset/duration line values.