你好!
需要将单组LVDS转成2组LVDS给1920X1080的10寸TFT用。请推荐下用什么型号的LVDS可以胜认?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
官网选型网页去找找吧.
http://www.ti.com.cn/lsds/ti_zh/interface/equalizer-products.page
可以参考DS10BR254这款,可以实现标清或高清信号扇出(SD/HD SDI Routers)这类应用。
你好,给你推荐一个比较符合你要求的高速率传输芯片 LVDS双路 最大传输速率3.2Gbps,带宽支持6-160mhz THCV231/236或者THCV25/236
THCV231可以将最高12Bit/pixel的LVCMOS并行信号转换为串行图像信号的发送端IC。最其具备大传输速率3.2Gbps的CML串行输出,可以将1080p60Hz的12bit摄像头图像信号通过一对双绞线或者一根同轴电缆进行传输。此外,可以通过双向的传输通道进行I2C信号传输。
THCV236/可以将THCV发送端IC输出的串行图像信号转换为最高32bit/pixel的LVCMOS并行图像信号的接受端IC。1080p60Hz的16bit的摄像头图像信号通过一对双绞线或者一根同轴电缆进行接收。此外,还具备一条可以用来传输I2C、UART或GPIO等串行信号的Sub-Link,向传输通道“Sub-Link" I2C/UART/GPIO(最高4条)
详细信息可看官网http://www.thine.co.jp/zh_cn/products/num_details/THCV231.html,我司可提供规格书、样片和技术支持,欢迎联系qq:2817821256 手机18682112448