Other Parts Discussed in Thread: TXB0101
自己做得PCB。一个芯片为3.3V 飞思卡尔k60串口,一端为AT89C52单片机串口,中间为TXB0101进行电平转换,5V往3.3V转换正常,3.3V转5V串口接受乱码,工作方式是测试---芯片通电---测试结束---断电。用FT232rl进行串口直连,收发正常,单独测试io引脚电平,转换正常,没有虚焊,变成串口5V那边收到乱码。有没有专门用作串口电平转换的芯片,谢谢、
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
3.3V 转5V时候,你看下3.3V 飞思卡尔k60串口的输出电流为多大?因为TXB0101 对输入有个要求:For proper operation, the device driving the data I/Os of the TXB0101 must have drive strength of at least ±2 mA.。
这种方法的的弊端就是电源间电流会互串,混合电压系统还是建议加上电平转换芯片最好。
Kailyn Chen 说:这种方法的的弊端就是电源间电流会互串,混合电压系统还是建议加上电平转换芯片最好。
各有各的有点和缺点。当然最大的缺点就是你所说的电流会互串,但是如果对精度要求不高的话,还是可以采用这种方案的。