电路中需要用SN74LVC1G04这个反相器,电源供电为5V。输入电平为单片机的输出,高电平为3.3V,低电平为0V。我看SN74LVC1G04的数据手册上写着,当供电电压为5V时,要求VIH大于0.7X5=3.5V。我想问输入高电平为3.3V,能否满足该器件的输入电平要求?官网写着该器件输入类型为TTL/CMOS,应该是支持3.3V高电平输入的,请帮忙尽快确认,谢谢!
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
电路中需要用SN74LVC1G04这个反相器,电源供电为5V。输入电平为单片机的输出,高电平为3.3V,低电平为0V。我看SN74LVC1G04的数据手册上写着,当供电电压为5V时,要求VIH大于0.7X5=3.5V。我想问输入高电平为3.3V,能否满足该器件的输入电平要求?官网写着该器件输入类型为TTL/CMOS,应该是支持3.3V高电平输入的,请帮忙尽快确认,谢谢!
我们产品特性以数据手册为准。这个器件是CMOS电平,不支持3.3V高电平,但器件会留有一些裕量,所以有可能可以工作。但出问题我们不能负责,因为已经超出了芯片spec。为保证可靠,建议替换为LV1T04。
我觉得要么按照Dylan的办法改成LV1T04,如果不好改芯片的话,看看方便不方便再加一片3.3V到5V的电平转换器件,这两种办法都比较保险。
按照SN74LVC1G04的DATASHEET,在VCC=5V供电的情况下,VIH=0.7VCC=3.5V<3.3V,按理是不可行的。
唯一的可能性就是,SN74LVC1G04的实际供电电压VCC 小于或者等于 4.7V,即实际的VCC=4.5V~4.7V,此时VIH=0.7VCC=3.15V~3.3V,系统可以正常工作。
若实际的VCC=4.7V~5.5V,则系统不可能正常工作的。
在大多数情况下,5V供电系统的实际电压一般都会低于5V的,所以LZ遇到的现象是很常见的(理论上不可行,实际应用中却可行)
SN74LVC1G04这个反相器我记得是不能支持3.3V高电平输入的吧。CMOS工艺的高电平需要是0.7*VCC=3.5V。
SN74LV1T04,这个器件5V工作电压可以接受最低2.03V高电平。希望对你有帮助。。
SN74LVC1G04能支持3.3V高电平输入,当供电电压为4.5V~5.5V时,Vih(min)=0.7Vcc,3.3V高电平输入的话,那么仅需要供电电压在4.5V~4.7V左右就好。但如果楼主的供电必须是5V的话,只能考虑SN74LV1T04这款了。
liming liang 说:电路中需要用SN74LVC1G04这个反相器,电源供电为5V。输入电平为单片机的输出,高电平为3.3V,低电平为0V。我看SN74LVC1G04的数据手册上写着,当供电电压为5V时,要求VIH大于0.7X5=3.5V。我想问输入高电平为3.3V,能否满足该器件的���入电平要求?官网写着该器件输入类型为TTL/CMOS,应该是支持3.3V高电平输入的,请帮忙尽快确认,谢谢!
SN74LVC1G04这个3.3V也可以工作,但是不稳定,推荐使用SN74LV1T04。
Ti逻辑器件的数据手册中负值代表的是流出的电流,正值代表的是流入的电流。
可以参考下这篇文章是关于“正确理解TI逻辑产品数据手册”的,里面对datasheet中各个电气参数都有详细介绍。