Part Number: DS90UB948-Q1
主 IIC输出的400Khz 经过 ds90ub941ASQ 到ds90ub948Q1 透传出来的IIC 只有76.9Khz .请问如何解决 透传中途会衰减 IIC 的速率问题。 
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Part Number: DS90UB948-Q1
主 IIC输出的400Khz 经过 ds90ub941ASQ 到ds90ub948Q1 透传出来的IIC 只有76.9Khz .请问如何解决 透传中途会衰减 IIC 的速率问题。 
您好,948的0x26和0x27您是怎么配置的?
在您的应用中MCU--DS90UB941--DS90UB948---Display,如果要和remote slave 通信,948作为代理控制器,948的I2C速度是通过0x26和0x27配置的。
默认的是100Khz的速率。
I2C_PERIOD = SCL_HIGH_TIME + SCL_LOW_TIME
I2C_FREQ = 1/I2C_PERIOD
以0x26默认值为0x83,0x27默认值为0x84为例,默认的是100Khz的速率,我们可以计算下。
0x83十进制=131,0x84十进制=132.,OSC内部晶振使用的是26Mhz

SCL_HIGH_TIME=(1/OSC)*register value=(1/26*10^6)*131
SCL_LOW_TIME=1/OSC)*register value=(1/26*10^6)*132
因此SCL_HIGH_TIME + SCL_LOW_TIME=(1/26 *10^6)*(131+132)
I2C_FREQ = 1/I2C_PERIOD=(26 *10^6)/263=100Khz