Other Parts Discussed in Thread: TUSB2046B, TUSB8040A, TUSB8040
TUSB2046B这个芯片是USB1.0还是USB2.0的呢,为什么在datasheet上没有说明啊
我们产品上需要一个USB HUB(1转4)支持USB2.0,请推荐合适的芯片
谢谢
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
datasheet中写了Full Speed 和low speed, Full speed是12Mbps速率,Low speed是1.5Mbps, USB2.0向下兼容,除了支持这两种速率之外,还支持480Mbps的高速速率。所以你说的想需要一个支持USB2.0的HUB,是不是指的480Mbps速率的?
你好
不是的,没有要求必须支持高速模式(480Mbps)。
那么对于这颗没有高速模式的IC,我们是否可以认为除了高速模式其余完全满足USB2.0的需求呢?
TUSB2xx系列的HUB其实都是遵循USB2.0的协议的,只是只能支持USB2.0的全速模式。(USB 2.0规定了3种速率模式,低速(1.5Mbps),全速(12Mbps),高速(480Mbps)).