我司现用FPD-LINK-DS90UB925来驱车载屏,一直没有信号输出,想请TI原厂支持,想要准确联系方式。谢谢
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
目前就是在输入正常的条件下没有输出是么? 把电路图传上来看下吧, I2C 时序正常吗?
现在就是我用RGB屏显示正常的数据和这个是并联结口,现在I2C没有和芯片通讯,是不是不用软件配置就可以用啊?帮忙分析一下是那的原因,谢谢!
不知道你这个问题解决了没有,如果没有,请测量下VDD33 , VDDIO和PDB的时序,datasheet中给出PDB一定要在VDD33和 VDDIO完全上电稳定之后1.5ms之后再起来,推荐这个引脚上拉10K电阻到VDD,并且需要接一个大于10uF的电容到地以保证有足够的延迟,并且所有的输入端也必须要在Vdds上电稳定之后再给输入。可用示波器量下时序看是否符合。
1.8V或者3.3V都没问题,主要就是为了和外围电路电平兼容,这样就省去了由电平不匹配带来的麻烦,或者还需要再加个电平转换类的器件,也增加板子空间,所以说这里的LVCMOS电路既可以用1.8V供电也可以用3.3V供电简化了电路设计,使用起来更加方便。