This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
如果只是简单的IO,并且变化速度很低的话,可以考虑简单的SN74AHC1G125这一类的buffer。如果速率在10Hz~1MHz的,就需要用差分逻辑来传输,可以考虑485芯片像SN65HVD08这一类,如果速度再高1M~500M,可以考虑用LVDS逻辑来传输,Sn65LVDS050这样的
您好 我这个是简单的IO, 那这么长的距离即使是简单的IO 用SN74AHC1G125去驱动的话 会不会驱不起来 譬如电压衰减之类的?
5米不算太远的距离,SN74AHC1G125没有问题的。不过它是单向的。要是单向可以的话,你使用普通三极管也可以啊