This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DP83865选用RGMII模式时,CLK_TO_MAC功能脚的设计,以及RGMII_SEL(1、0)脚的配置问题

1)在RGMII模式下,CLK_TO_MAC引脚一定要连接到MAC芯片么?如果不连接会有什么影响?我选用的是ARM芯片,其内部有自带的MAC模块,与DP83865进行通信;

2)MAC接口形式的配置,GRMII_SEL1和RGMII_SEL0的配置,可以决定其模式,请问手册中提到,GRMII_SEL1=1,GRMII_SEL0=1时,为RGMII-3COM模式;GRMII_SEL1=1,GRMII_SEL0=0时,为RGMII-HP模式,这两种RGMII模式有什么区别,一般都配置成哪种模式?