This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DP83640驱动

Other Parts Discussed in Thread: DP83640, DP83640SW-LIB

在课题设计中,使用DM9000与DP83640连接,请问DP83640的驱动如何开发,可以使能1588功能。新手,希望大神能详细指导一下

  • 请问你计划用什么处理器? 跑什么系统呢?

    软件设计方面有个例程可以参考: http://www.ti.com.cn/tool/cn/dp83640sw-lib?keyMatch=DP83640&tisearch=Search-CN

    DP83640的1588功能的使用可以先看看以下几个应用笔记:

    • IEEE 1588 Synchronization Over Standard Networks Using the DP83640 
    • IEEE 1588 Boundary Clock and Transparent Clock Implementation Using the DP83640  
    • IEEE 1588 Synchronization Over Standard Networks Using the DP83640 (cn)  
    • Application Note 1729 DP83640 IEEE 1588 PTP Synchronized Clock Output (cn) 
    • IEEE 1588 Precision Time Protocol Time Synchronization Performance (cn)  
    在以下网页也下载:
    http://www.ti.com.cn/product/cn/DP83640/technicaldocuments


  • 我使用的是三星的S3C4251的ARM9芯片,跑的是Linux系统。第一次做这种项目,不懂的太多。所以想理清一下开发的步骤和一些学习资料。谢谢你,我看看上面的资料

  • 您好,小弟最近在研究dp83640,但是时间戳寄存器读不出值,其他寄存器都可以,不知道是什么原因啊

  • 你好 最近也在研究DP83640 可以一起交流一下吗?

  • 您好,我想问下DP83640 软件设计和 C 软件参考库,如何获取呢