最近在研究dp83640芯片,配置的是光口接受,光口插上灯是闪的,而且在MII接受断也有反映,应该是收到数据包了。用STM32配置DP83640的,通过SMI接口读写寄存器,现在的情况是,读写其他寄存器都可以,芯片也有反应,但是读取recieve_timestamps寄存器读出来老是0,PTP_RXCFG1配置好了,PTP_RXCFG3中的自动打时间戳功能也是关闭的,然后读取状态寄存器PTP_STS寄存器的RXTS_RDY的值是1,配置RXTS_IE中断也能产生相应的中断,但是中断是一直拉低的,说明芯片一直是在准备接受时间戳,请问如何才能正确配置芯片才能接受时间戳??????