你好!
DS90UH927Q规格书中提到支持AC-Coupled STP Interconnect up to 10 Meters,请问这是基于什么样的线材才能达到10M的传输距离?
我们现在用的是DS90UH927Q发送,DS90UH928Q接收。传输1280*720分辨率的视频数据。这样的配置如果需要传输5M的距离,需要什么规格的线材?
以上
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
单纯来说超5类线能够支持的最大有效距离5m肯定没问题,但是对于DS90UH927Q的线材要求是屏蔽双绞线,并且实验已经验证:Bit error rate testing
of input to the serializer and output of the deserializer with 10 meter cable shows no error when the noise frequency is less than 50MHz。
Cable的传输距离 和cable(单位距离的在1.5GHz信号的衰减量)、connector(插损)、PCB Layout走线都有关系,附件是TI验证过的cable和connector供您参考,同时还有PCB layout走线建议。