This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

RS485(SN64LBC184)在实际使用中出现问题!!!!!

各位好,这边有一个项目,有一个485通信控制器,有8个通道,每个通道挂32个485终端,距离应该在300M以内,速率在19200,

现在出现这样的问题,在刚开始使用的时候,通信都正常,但用了一段时间就出现通信很差,终端的数据一直重传,导致整个系统

运行不畅,当出现这个问题之后,我软件重起我的485通信控制器,通信会好一点,但我直接把485通信控制器硬件关机(关掉电源)一段时间

在上电,就可以正常运行一段时间,但过几个小时又出现之前的问题!

我的理解是485通信的AB线的共模电压太大的原因,不知道各位是否有好办法!!

谢谢!