Y输入一个50Khz占空比是5%的波形。AB脚的波形是这个样子。我用的是567脚。PCB版图:
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
您具体是什么应用?是RS-485 或 RS-422应用吗?您可以附上完整的电路图吗?包括接收端电路,使用的是什么芯片?
如果您使用的是16-Pin 封装的 AM26C31,其8脚是GND,如下管脚定义,我不明白您为什么在8脚和6脚之间焊了一个120欧姆的电阻,我想您是不是把管脚定义弄错了?
现在在另一个产品上也用到了这个芯片,它的3脚电压输出太低,不到1V。这个产品我用的是1脚2脚3脚 .其中2脚电压正常。3脚电压太低。不到1V。以至于2脚和3脚之间的压差只有2V左右,不到3V
差分输出2V是在datasheet 规格范围内的,如下截图,这里也建议您附上完整的电路图,包括接收端电路,以作分析。这里1脚2脚和3脚的波形是怎样的?也建议附上看下
Y输入一个50Khz占空比是5%的波形。AB脚的波形是这个样子
这里描述的Y和AB脚是指的U8管脚的定义吗?还是指U21 AM26C31的A输入,YZ差分输出?因为您的问题是关于AM26C31的,而您描述的却是U8 管脚的信号,这里有些不清楚,请您澄清一下。
J2看上去是一个connector,并不是 receiver(接收器),120Ω电阻应接在接收器的差分输入端。
关于另一个产品,您可以去掉上拉和下拉吗,加终端电阻测试其输出信号?;3脚应该输出低电平,现在输出3V至4V应该是被5V上拉上去的。
很高兴您第一个产品的问题解决。
关于另一个产品,您是去掉的R9和R10吗?3脚输出3V至4V的电压是异常的,测试时是否加了终端电阻?
芯片是否已经损坏?换一个AM26C31再试试呢?