HI 版主:
TFP410是否可以把从DVI接口接收到的数据直接显示到LCD屏上?
对于不同大小的屏,TFP410直持分辨率的自动调整吗?还是需要通过I2C总线去设置?
因为我现在在找一款这样的芯片:
1。 要求input支持VGA信号输入,output 数字信号输出
2,。支持1024x768,1366x768,1600x1080,1920x1080等多种输入分辨率
3。 输入的VGA信号可以动态识别。
多谢!
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
找到了TVP7002,但不知道是否支持VGA信号输入分辨率的自动识别?