Other Parts Discussed in Thread: DS90UB914A-Q1
TI工程师们好!
请问一下在ESD干扰的环境下,LVDS IC有可能发生复位吗?(DS90UB914A,DS90UB928Q)
1、单纯的LVDS输入或其它某个IO口的受扰会有复位可能吗?
2、913和914之间是否支持同轴线传输,或者有没有更好的线材推荐?
以上,谢谢
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Other Parts Discussed in Thread: DS90UB914A-Q1
TI工程师们好!
请问一下在ESD干扰的环境下,LVDS IC有可能发生复位吗?(DS90UB914A,DS90UB928Q)
1、单纯的LVDS输入或其它某个IO口的受扰会有复位可能吗?
2、913和914之间是否支持同轴线传输,或者有没有更好的线材推荐?
以上,谢谢
DS90UB914A-Q1的ESD等级是IEC 61000-4-2,它是芯片级别的ESD等级
你的板子在ESD干扰下是系统的ESD等级,和芯片的ESD等级不太一致的
我现在不是想了解ESD等级的问题。
而是在LVDS信号受干扰的情况下,是否会引起芯片复位。
使得其复位的条件有两个:1)PDB引脚为low电平的时候,器件进进入shutdown模式,内部寄存器reset恢复到默认值。2)就是power on reset的内部寄存器0x01使得器件内部模拟和数字模块都将reset。你说的收到干扰一般不会导致复位。