TSB82AA2支持使用两线制的EEPROM配置寄存器。在datasheet里提到,如果不使用EEPROM,SCL管脚通过220Ω电阻下拉。
如果不使用EEPROM,如何配置对应寄存器?(器件手册第七节: initialize the 1394 global unique ID register and a few PCI configuration registers)
如果使用EEPROM,手册里要求使用完成编辑的,TI有提供软件编辑EEPROM吗?
The TSB82AA2IPGEEP sopports a 2-wire EEPROM to configure its registers after power on reset. But in the datasheet, also has that " ROM is not implemented. Connect terminal 3(SCL FOR EEPROM) to ground with a 220-Ω resistor." My question is that, if I do not use the EEPROM, how can I initialize the 1394 global unique ID register and a few PCI configuration registers? If I use the EEPROM, does TI support a software to program the EEPROM?