我在一个UWB高精度定位系统里边,需要设计定位基站的时钟同步电路,具体是由恒温晶振输出10MHz的LVCMOS信号,输入给时钟综合器,最后输出38.4Mhz的信号。一开始打算用FPGA通过PLL倍频分频实现,后来了解到有这样的时钟发生、及相应的缓冲分配、抖动消除等电路,请问这两种方法哪个更好一点?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
你要求几路输出?要求的jitter是多大?LMK03806,6208等都可以实现
要求是四路以上输出,通过双绞线传输最多100m的距离,传输距离较远,只能是差分输出吧。输出相位噪声有要求:-132dBc/Hz @1KHz ,-145dBc/Hz@10KHz。
输出38.4Mhz主要用于UWB定位系统中的接收机时钟同步,接收机相隔几十米,采用有线传输时钟信号给定位接收机使用。我采用WeBench软件实验了几次,觉得LMK02002和LMK04821_VCO1可能会满足我们要求的相位噪声。这两款芯片都要求片外VCO,是不是会大幅增加成本呢。
不推荐用LMK02002系列。你可以看看LMK0480x系列和LMK04906,会比4821便宜一些。外部的VCXO肯定会增加成本的。
使用双环的话,第一个实现抖动清除,第二个实现时钟合成。而我的输入参考信号是OCXO输出的LVCMOS电平,信号质量很好。我觉得使用单环PLL就可以了。我这样理解对不对?
是的,你理解的完全正确
单环的,你也可以看看LMK03806等03系列的产品,这个是单环的