This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

RS-422 and RS-485 接口芯片选择

Other Parts Discussed in Thread: ISO3086, ISO3082

你好,

   我需要建立两条总线,请给出应该选择芯片的型号,要求如下:

一条RS-422总线:+5V供电,+5V信号电平,最大64个节点,要有故障保护功能,全双工但要求发送可控,速率≥2Mbps ,温度范围为工业级-40℃—70℃。可以是单独一个芯片,也可以收发分开为两个芯片。

一条RS-485总线::+5V供电,+5V信号电平,最大64个节点,要有故障保护功能,半双工,速率≥2Mbps,温度范围为工业级-40℃—70℃。

请给出最适合的芯片选择,并请优先给出长期不会停产的芯片型号。

谢谢!祝工作愉快!

  • 一条RS-422总线:+5V供电,+5V信号电平,最大64个节点,要有故障保护功能,全双工但要求发送可控,速率≥2Mbps ,温度范围为工业级-40℃—70℃。可以是单独一个芯片,也可以收发分开为两个芯片。

    *********************************************************************************************************

    如果现场需要隔离接口,请考虑ISO3086,可以支持到20Mbps的速率,详细资料查看如下链接 www.ti.com/.../iso3086

    *********************************************************************************************************

    一条RS-485总线::+5V供电,+5V信号电平,最大64个节点,要有故障保护功能,半双工,速率≥2Mbps,温度范围为工业级-40℃—70℃。

    *********************************************************************************************************

    如果现场需要隔离接口,请考虑ISO3082,可以支持到20Mbps的速率,详细资料查看如下链接  www.ti.com/.../iso3082

    *********************************************************************************************************

  • 如果现场需要隔离接口,请考虑ISO3086,可以支持到20Mbps的速率,详细资料查看如下链接 www.ti.com/.../iso3086

    能问下,RS422使用ISO3086后可以最大接64个节点吗?

  • haiyan niu 说:

    如果现场需要隔离接口,请考虑ISO3086,可以支持到20Mbps的速率,详细资料查看如下链接 www.ti.com/.../iso3086

    能问下,RS422使用ISO3086后可以最大接64个节点吗?

    RS422和RS485的区别在于二者的总线架构不同,RS422是multidrop架构,也就是总线上一个driver,多个receiver,标准的RS422总线上最多可挂接10个receivers。 RS485为multipoint架构,多个driver和多个receivers,最多挂接节点数根据unit load,ISO3086为1/8 unit load,最多可挂接256个nodes。