This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TS3DV642: 接入HDMI,信号D+和D-交换交换极性接

Part Number: TS3DV642


咨询一个TS3DV642问题,使用该器件做HDMI切换开关,HMDI信号一定要按照TS3DV642的引脚定义D+和D-对应关系接吗,例如能否D+接到HDMI-信号上,D-接到HDMI+信号上,以此组成差分对
我的理解从手册上看应该是可以的,芯片架构图示就是开关
为什么要这样做的原因是,下图的5、6、7、8、10、11、12、13边的组合接到常规贴片的HDMI Connecter是必须要打过孔的,加上CPU到TS3DV642也要打过孔,HDMi信号上的过孔会非常多,到时HDMi眼图会很差