This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
通信后,A和B,如果同时供电后,无法正常485传输数据,这个是什么情况,如果单独供电后,可以传输。
您好,
很抱歉没明白您的意思,A和B是 SN65HVD3082E的差分接口,为什么要同时供电?
还是说A和B是指485节点,两个节点同时供电485总线不能正常通信?如果是这样的话,看下是否同时供电,供电电源输出功率不够造成的?
您好,是2个设备,485对接传输设备。有的时候无法传输
根据您的问题描述,我在网上找到如下问题,应该与您的问题一致:
集中供电的RS485系统在上电时常常出现部分节点不正常,但每次又不完全一样。这是由于对RS485的收发控制端TC设计不合理,造成微系统上电时节点收发状态混乱从而导致总线堵塞。改进的方法是将各微系统加装电源开关然后分别上电。
解决办法一个是分别上电微控制系统,就是您说的方法单独供电;另一个是收发器控制端微控制器引脚通过反相器控制,而不采用MCU引脚直接控制以防止MCU上电时对总线的干扰,如下截图所示: