This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DS90UB941AS-Q1: 941的GPI和948的GPO映射关系是否必须一一对应

Part Number: DS90UB941AS-Q1


当941的GPIO1设置为input,948的GPIO1设置为remote output,可实现GPIO的透传。

请问下,是不是必须 941_GPIO1===948_GPIO1、941_GPIO2===948_GPIO2.......这样一一对应?

可不可以配置成交叉的方式:941_GPIO1===948_GPIO2 这样?

Thanks!