Hi:
目前使用TCA9548碰到一个问题,VCC供电原为3.3V,23、22pin SDA、SCL上拉电压为3.3V,输出端SCL0~SCL7、SDA0~SDA7上拉电压为1.8V。
测试SCL0~SCL7与SDA0~SDA7波形,发现波形的高低电平均被抬高。低电平约400mV,高电平约2.1V。通过再次阅读手册,"For example, if the main bus is running at 5 V and the downstream buses are 3.3 V and 2.7 V, Vpass must be equal to or below 2.7 V to effectively clamp the downstream bus voltages.",且根据Figure14,确定为Vpass电压不满足要求,3.3V VCC供电下,Vpass电压约2V。
后续改版想将VCC供电电压降为2.5V,其余不变。如下图:

理论上来说,2.5V VCC供电,对应的Vpass电压约1.8V。但我不确定输入端的上拉电压为3.3V,这样的应用是否正确呢?