This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DS125MB203: CH0和CH2通道的VOD/DEM参数调整寄存器是哪个?

Part Number: DS125MB203


当前A通道有少量调度(10GE业务),很想知道的CH0 NC – S_INA0 和CH2 NC – S_INA1通道的VOD/DEM调整寄存器是哪个?还是默认不可调?另外INA0/1输入端我使用了10nf耦合电容,不知是否需要使用100nf电容?(10nf的高频性能要优于100nf)

  • 更正:当前A通道有少量丢包(10GE业务),很想知道的CH0 NC – S_INA0 和CH2 NC – S_INA1通道的VOD/DEM调整寄存器是哪个?还是默认不可调?另外INA0/1输入端我使用了10nf耦合电容,不知是否需要使用100nf电容?(10nf的高频性能要优于100nf):

    补充:slave模式,0x5e配置为0x7;0x5f配置为0xf2

  • 很想知道的CH0 NC – S_INA0 和CH2 NC – S_INA1通道的VOD/DEM调整寄存器是哪个

    您好,0x0F和0x1D这两个寄存器是CH0 NC – S_INA0 和CH2 NC – S_INA1的EQ控制。这两个通道是输入端,所以只有EQ控制。

    DEM和VOD指的是输出端的配置。

    另外INA0/1输入端我使用了10nf耦合电容,不知是否需要使用100nf电容?(10nf的高频性能要优于100nf)

    通常AC耦合电容的大小选择100nF。