This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TCAN1145-Q1: 输出脚12/13脚没有信号, 电平为0

Part Number: TCAN1145-Q1

hi Ti Engineer

有几个项目用到用到1145,之前用的是NXP的TJA1145T,现在我们想都换成TCAN1145DRQ1,对比了二种芯片的规格书,没有发现什么不同。 现在在一个新项目(热管理)上用,发现该芯片无法正常工作,直接换成TJA1145T(PCB上预留了二种封装)工作正常。 相同电路板硬件完全一样、相同MCU程序,都不接外设,工具万用表和示波器,TCAN1145DRQ1 的TXD脚能看到MCU发的信号,输出脚12/13脚没有信号, 电平为0。换成TJA1145T一切正常。比较二种芯片引脚状态,除了12/13脚不一样(TJA1145T的12/13脚 2.5V、TCAN1145DRQ1的12/13脚 0V)其他引脚 都一样。 初步排除焊接问题(通过测量电阻值比较),并也更换了几片TCAN1145DRQ1验证,状况还是一样的;请帮忙看下哪里有问题?