This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DS90UB960-Q1: 看不到I2C地址

Part Number: DS90UB960-Q1
Other Parts Discussed in Thread: TPS4H160-Q1

我有一个同事为xavier jetson agx 核心板设计了一块接口板,交给我来调试。其中一个接口是四路摄像头连接四个ds90ub953(这个是购买的成品),我的理解是视频信号被953编码后通过同轴电缆进入接口板,接口板内有960解串器,解串后进入xavier 核心板。同时为960配置一个TPS4H160-Q1 40V、160mΩ 四通道智能高侧开关,我的理解是类似于供电。但是现在xavier的I2C总线探测不到960的地址,我的问题是:

1、这种设计思路是正确的么?如果不正确,应该怎么改。如果正确的话,为什么看不到地址?

2、同轴电缆连接的接口,我的xavier能看到953的I2C地址么?因为摄像头厂家说要通过I2C对953进行配置。

3、960芯片是否有驱动文件需要在核心板中加载?

4、高侧开关的作用是什么?是否可以取消?

5、我看960的手册里面典型应用中给I2C总线设计了电压和电阻,请问这个是必要的么?

6、我们的960接线。

本人新手,希望回答尽量详细一点