Other Parts Discussed in Thread: DS90CF383B
您好,如下所示原理图设计,使用DS90UB947串行和DS90UB948解串回环检测信息出现错位问题,该现象可能是什么原因导致呢,


This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
您好,如下所示原理图设计,使用DS90UB947串行和DS90UB948解串回环检测信息出现错位问题,该现象可能是什么原因导致呢,


RGB data mapping配置方式这边已经确认过是对得上的,然后引脚也是按照datasheet来的,请帮忙确认DS90CF383B手册的RGB信号引脚是否无问题,这边无法从软硬件方面找到原因
谢谢,错位已找到原因是RGB data mapping的问题,本来是OpenLDI Mapping结果变成
SPWG Mapping导致RGB错开两位,但是我已经通过分压电阻把MODE_SEL1定成OPENLDI mapping,为什么还会出现这种情况,必须要配置寄存器要修改吗(图中NC表示不焊接)
通过strap pin MODE_SEL0和MODE_SEL1来进行配置就可以,寄存器默认值也是strap pin的配置。
只有配置OLDI dual pixel模式还是single pixel模式的时候,0x4F[6】的值是和strap pin相反的。