Part Number: TCAN4551-Q1
Other Parts Discussed in Thread: TCAN4550
有个问题请教下,这句话的意思是:如果用1.8V的IO电压,就不能用晶体对么?
那没有外部时钟,又想用1.8V的VIO,是否可以挂一颗1.8V供电的TCXO?如果不行的话,有没有其它办法可以满足我这种应用要求?谢谢!
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Part Number: TCAN4551-Q1
Other Parts Discussed in Thread: TCAN4550
有个问题请教下,这句话的意思是:如果用1.8V的IO电压,就不能用晶体对么?
那没有外部时钟,又想用1.8V的VIO,是否可以挂一颗1.8V供电的TCXO?如果不行的话,有没有其它办法可以满足我这种应用要求?谢谢!
:如果用1.8V的IO电压,就不能用晶体对么?
是的,如果1.8V IO电压,则不能使用crystal来提供时钟。
这是因为3.3V 或5V 的 VIO 电压时、TCAN4550和 TCAN4551这两款都支持crystal提供时钟源。TCAN4551是 TCAN4550的简化功能版,也经过修改以支持1.8V 的数字接口电平。
内部时钟电路和数字电路都是使用VIO供电,所以当1.8Vio供电时,内部时钟电路没有足够的电压来正常工作,必须将外部单端时钟信号用于时钟源。 此外部时钟源应直接输入 OSC1管脚,且 OSC2管脚必须接地。