Part Number: DP83825I
pin2和pin4是strap pin,从芯片出来串联一个0Ω电阻,然后接到RJ45连接器上的两个指示灯(RJ45连接器两个指示灯的电路是一样的)。我们想用的就是pin2和pin4的默认低电平(Pin 20 is configured as CRS_DV;Auto Negotiation Enable),但是在调试过程中,发现pin4不是低电平,被拉高了,导致接10M网口时,不能识别。想问下是不是芯片里面电路有差别
下图是RJ45连接器内部模型,9和12接的是3.3V,10和11分别接到DP83825I的pin2和pin4