This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DS90UB960-Q1: 与 ds90UB913配对使用 传输YUV8bit数据 是否可行

Part Number: DS90UB960-Q1


您好,计划使用DS90UB913A + DS90UB960 方案,

数据流:camera端,ISP 输出YUV 8bit 到 913a,960 csi接口输入至SOC;

问题:根据spec,960连接913工作在raw mode,请问此模式下能否传输YUV 8bit数据,上述方案是否可行;

 (在关联的论坛中提到 960 0x70寄存器设置为0x1E是YUV 8bit data,但spec中未查询到) 

  • 在关联的论坛中提到 960 0x70寄存器设置为0x1E是YUV 8bit data,但spec中未查询到

    您好,这个在MIPI CSI-2协议规范中给出data code。比如:

    YUV422 8-bit = 0x1E

    YUV422 10-bit =0x1F

    RAW8 =0x2A

    RAW10=0X2B

    960连接913工作在raw mode,请问此模式下能否传输YUV 8bit数据,上述方案是否可行;

    是的,和913/933搭配使用时,只能工作在RAW  mode。所以是不能传输YUV 8数据的。