Other Parts Discussed in Thread: TS3V712EL, TS3V713EL, TS3V712E
我需要一个2路VGA信号输入至1路VGA信号输出的选择芯片,请问使用TS3V712E可以吗?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
首先这几款都可以用做VGA的开关,并且都是2选1的,不过它是7个通道的,每个VGA device包含7个视频信号(R, G, B,HSYNC, VSYNC, DDC CLK, and DDC DAT),如果你的应用中只有RGB信号,或者RGB,加上两个同步信号,也都是可以用的,注意不用的A端的口直接接GND,B端的可直接悬空即可。
那为什么在TS3V712EL和TS3V713EL的数据手册中都写的是“7-channel video demultiplexer for switching between a single VGA source
and one of two end points. “,而在TS3V712E中写的是“7-channel video multiplexer/demultiplexer for switching between multiple
VGA sources or end points. ”。看意思是TS3V712EL和TS3V713EL适用于1个输入源对2个输出的显示终端,是1:2的选择。而我现在需要的是两个输入源只有一个输出显示终端的2:1结构,还请再次帮助确认一下TS3V712EL和TS3V713EL是否合适,因为这两款价格比较便宜,谢谢!
这几款功能相同,都是双向使用的,因此同样适用于2选1的多路选择。TS3V712EL和TS3V713EL内部都集成了HSYNC和VSYNC的电平转换,这样如果电平不匹配的话,就不需要额外再加器件了。
TS3V712EL是2选1的视频开关器件,由使能端SEL的高低电平决定哪个通道导通,比如当SEL=L时,R1,G1,B1的开关闭合,说明和R1,G1,B1的导通,也就是说R0,G0,B0的输出的是R1,G1,B1。同理,SEL=H时,R0,G0,B0的输出的是R2,G2,B2。
hui liu9 说:请问一下该芯片2输入转一输出的详细原因,没看懂pdf的描述,麻烦您了