This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
DS160PR410 EVM提到的下载器USB2ANY,必须使用USB2ANY下载器吗?手上有TI的 USB Interface Adapter(电源PMBUS用的),可以用来配置 DS160PR410吗?
1、USB2ANY和 USB Interface Adapter两个下载器都是USB转I2C,有什么区别,可以通过软件升级相互 替换吗?
2、DS160PR410在按照EVM的电路设计后,上电不操作任何寄存器,它的redriver功能会正常使能吗?
您好,
1、USB Interface Adapter属于电源产品,我不了解它的应用,看它的用户指南还需要安装 transport DLL driver 和 GUI demo software,与USB2ANY不同,我再确认下这个问题。
2、DS160PR410可以通过不同的方法来配置((SMBus 或 I2C、EEPROM、pin mode),如果不操作寄存器可以使用pin 模式。