This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DS90UB936-Q1: 如何监控936与Serializer之间FPD-LINK的信号质量

Part Number: DS90UB936-Q1

主机端使用的Deserializer是ds90ub936,摄像头端使用的Serializer是ds90ub933。

发现有的摄像头接入主机后可以出图,有的不能出图;而不能出图的摄像头接入其它主机也可以出图。

不能出图时,我们测量了936的CSI、933的DIN都没有问题,从936的4D寄存器看LOCK_STS=1、PORT_PASS=1,即FPD-LINK是LOCK状态。

但是 0x22寄存器的FWD_SYNC0=0,0x35寄存器的TX_PORT_SYNC=0,0x73-0x75寄存器均为0,即936没有收到有效的video frame。

1、综上,我们怀疑是FPD-LINK的信号质量可能处于临界状态,是否有方法可以监控信号质量呢?

2、我们尝试了AEQ_RESTART=1重启AEQ,依然无法出图,是否说明AEQ对此已经无能为力了?

3、是否有手段来提升FPD-LINK信号的质量,比如“预加重”之类的?

Thanks!