This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
您好,
下面箭头所指的差分对是互连的吗?因为看到一个是TypeC_DP1/TypeC_DN1,一个是TypeC_DP1/TypeC_DN2:
EQ级别您是怎样设定的? 一般建议从EQ级别0开始,然后提升至EQ级别1,依此类推。为了使TUSB211识别对EQ设置的任何更改,必须切换RSTN针脚。 这是因为EQ引脚在通电时锁定,此后该引脚将被忽略。此外,TUSB211不会补偿信号路径中的任何直流衰减。 因此,建议在系统设计中尽量减少直流损耗(即电阻)。 因此,这可能会导致线路电容增加。 这是可以接受的,因为TUSB211可以补偿额外的电容负载。
您是否按照datasheet 8.2.2描述的步骤测试的USB眼图?