936的的FPD-LINK有两路RIN,
1. 是否可以支持同时接入2MP/30fps的摄像头呢?
2. 是否可以支持接一路5MP/30fps的摄像头?
麻烦贴一下是如何计算的。谢谢!
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
936的的FPD-LINK有两路RIN,
1. 是否可以支持同时接入2MP/30fps的摄像头呢?
2. 是否可以支持接一路5MP/30fps的摄像头?
麻烦贴一下是如何计算的。谢谢!
您好,936的each lane最大能支持1.664Gbps,4lane一共能支持6.656Gbps.
但936的CSI-2的带宽每个RX port只能支持到2.528Gbps 。
是否可以支持同时接入2MP/30fps的摄像头呢?
这就需要计算2MP/30fps的data rate 是否超过2.528Gbps。
2MP是1600*1200, 不知您使用的数据格式或色深是多少,假如RGB888 24bit格式,
那么total data rate为1600*1200*30*24*(1+25%)=1.728Gbps. 小于每个RX port能支持的2.528Gbps,所以是可以支持的。
是否可以支持接一路5MP/30fps的摄像头?
您的意思是使用1路,4lane,而不是2路,2lane输出配置方式是吗?